Implementation of EnDat
The EnDat interface is typically implemented in four stages:
- Realization of the “physical layer”; i.e. timing, “bits and bytes,” etc.
- Communication on the basis of mode commands
- Realization of complex processes, for example memory access
- Integration of EnDat communication in the controller structure
HEIDENHAIN provides various aids for the individual implementation stages:
- Documentation
- EnDat demo kit
- EnDat master
In the following you will find an overview of these aids and how they are used in the individual stages of implementation.
Documentation:
EnDat Technical Information:
The Technical Information provides a first overview of the EnDat performance. It summarizes the essential features of EnDat concisely.
Overview of EnDat documents
Overview of EnDat documents:
FAQ:
The FAQ area lists all information that we frequently discussed with our customers in the past.
FAQ area
EnDat Specifications:
The EnDat specifications contain detailed information on the physical interface, the timing and the data contents that are transmitted. This information is required for the implementation of the EnDat interface in subsequent electronics. For more information, please refer to your contact person at HEIDENHAIN.
EnDat Seminar:
The EnDat seminar provides detailed information about the different aspects of the EnDat interface:
- EnDat specifications
- Information on cables and connecting elements
- Information about the EnDat master
- Practical exercise in communication with EnDat encoders via mode commands
- Information on online diagnostics, datum shift, ...
The topics stated above are discussed using the "EnDat 2.2 Workbook", which provides compact information on all topics (including the EnDat specifications).
For more information, please refer to your contact person at HEIDENHAIN.
Application Notes:
Contain supplementary information on the specifications regarding the following topics:
- Structuring of mode command sequences
- Online diagnostics
- Zero point shift
- Handling of incremental encoders
- Implementation example
- Implementation of mode commands
- Implementation test
EnDat Demo Kit:
The EnDat demo kit is intended, on the one hand, for demonstration of the capabilities of the EnDat interface and, on the other hand, for communication with EnDat encoders on the basis of mode commands. The EnDat demo kit thus supports the design process in the following way:
- First, communication via mode commands can be tested outside the control loop
- It can be used as a reference in the course of integration of the EnDat master into the control loop
- Service for encoders together with the ATS software
The EnDat demo kit consists of the following components:
- IK 215 (PCI card for connecting EnDat encoders)
- EQN 1337 (multiturn rotary encoder)
- Cable: EQN 1337 à IK 215
- Software on CD
For more information, please refer to your contact person at HEIDENHAIN.
For more information, please refer to your contact person at HEIDENHAIN.
EnDat Master:
The EnDat master communicates with EnDat encoders from HEIDENHAIN. This allows simple transmission of position data and additional information to the superior application. The EnDat master can be integrated by means of a micro controller (µC) or an FPGA (Field Programmable Gate Array) or ASIC.
The µC solutions are used if the intended clock frequencies are relatively low. For µC integration, HEIDENHAIN offers an example code for the implementation of the EnDat 2.1 mode commands; for more information, please refer to your contact person at HEIDENHAIN.
Integration in an FPGA or ASIC is selected primarily for high transmission frequencies with purely serial data transfer. Different variants are available for integration in an FPGA or ASIC; the following graphic shows the block diagram for the EnDat master variants:
- EnDat Master Standard
- EnDat Master Reduced (only EnDat Protocol Machine)
- EnDat Master Light (only EnDat Protocol Machine)
EnDat Master Standard:
Due to the purely serial data transfer, an FPGA or ASIC is sufficient as master for the implementation of the EnDat 2.2 interface in subsequent electronics. To simplify the integration of the EnDat master in subsequent electronics, MAZeT (www.mazet.de) developed an EnDat master soft macro (EnDat Master Standard) with the following features:
- Encapsulated code block tested by HEIDENHAIN
- The implementation of the code block is secured through test vectors
- Designed for a short time to market
- All EnDat encoders from HEIDENHAIN are supported
More information and documentation can be obtained from MAZeT:
- EnDat master soft macro information sheet (insert link)
- EnDat master soft macro documentation
- EnDat master soft macro software examples
For more information, please contact MAZeT(www.mazet.de)
EnDat Master Reduced:
- Only the pure EnDat functionality (EnDat Protocol Machine) is integrated
- All EnDat encoders from HEIDENHAIN are supported
- Time to market unfavorable in comparison with the EnDat master standard version, as extended tests are required
- It does not offer further support regarding the convenient handling of the code or a micro controller interface
- Due to the restricted functionality, the code size is smaller than of the EnDat master standard version
- The code was tested only in an example application
- A concise documenation is available
For more information on applications of the EnDat master reduced version, please refer to your contact person at HEIDENHAIN.
EnDat Master Light:
- VHDL example code that only covers part of the EnDat functions
- Supports only absolute EnDat encoders, no incremental and battery-buffered encoders
- Time to market unfavorable in comparison with the EnDat master standard version, as extended tests are required
- Only the position is transferred in purely serial operation, no additional EnDat information
- It does not offer further support regarding the convenient handling of the code or a micro controller interface
- The code size is significantly smaller compared with the standard and reduced variants
- T he code was tested only in an example application
- A concise documenation is available (English only)
The EnDat Master Light can be provided at no charge as example VHDL code. Please refer to your contact persons at HEIDENHAIN.
Stages of implementation and associated aids
|
Realization of the physical layer
The EnDat specifications provide an exact description of timing and the “bits and bytes.” The EnDat specifications help you perform the entire implementation. MAZeT offers the FPGA soft macro, which completely covers the realization of the physical layer. HEIDENHAIN has tested the soft macro and recommends it for the implementation of the EnDat interface. The use of the EnDat soft macro reduces the developing time (time to market) and ensures error-free communication. This also minimizes the time needed for testing. For more information, visit www.mazet.de/produkte/sensorinterface_ics/endat/de. |
|
Communication on the basis of mode commands
Communication between the NC control and the EnDat encoder is based on the “mode commands.” In a second stage of implementation, the mode commands are used to set up basic communication with the encoder. HEIDENHAIN offers an EnDat demo kit consisting of a PCI card, a rotary encoder, cables and software. The provided software makes it possible to transmit individual commands to the encoder. The customer can very simply add a “low-level” application software to test the mode commands together with the EnDat master soft macro. Communication is based on simple register access. |
|
Realization of complex processes, for example memory access
The third stage of implementation then requires processes that comprise the transmission of multiple mode commands. These processes then include more complex tasks such as memory access. The annex of the EnDat specifications includes flowcharts that explain the required steps in detail. The same processes are available as example programs in “C” for the EnDat soft macro from MAZeT. |
|
Integration of EnDat communication in the controller structure
In the last stage of implementation the processes must then be integrated into the controller structures. |