Press releases and professional articles for journalists and editors

HEIDENHAIN develops, manufactures, and sells components for the core industries of machine tools, electronics, and automation. We also offer extensive press information for other product fields and industries.

Contact us directly if you have a specific question or wish to be added to our press mailing list: presse@heidenhain.de

HEIDENHAIN Testing and Inspection Equipment – Two devices, many practical possibilities for analysis

HEIDENHAIN encoders provide all of the information necessary for commissioning, monitoring, and diagnostics. So it is good if this data is quickly and easily usable during routine operation. With the PWT 100 testing device and the PWM 21 inspection device from HEIDENHAIN, specialists for the repair and maintenance of machines and facilities have many highly practical options for displaying and evaluating this comprehensive information as well as for analyzing the encoders.

The PWT 100 is a device for functional testing and adjustment, and the PWM 21 is an inspection unit for the diagnosis and adjustment of HEIDENHAIN encoders. Both units feature simple operation thanks in particular to the easily understandable way in which the results are displayed. They offer uncomplicated support for the commissioning, adjustment, monitoring, and diagnosis of all HEIDENHAIN encoders. Thanks to periodic and free firmware and software updates, the devices are always on the cutting edge of technology, and can test and inspect both current and future generations of encoders.

PWT 100: the portable testing device for adjustment and functional testing
The PWT 100 was designed to be used portably for the functional testing of HEIDENHAIN encoders on-site in production machines and facilities. For this purpose, it features a compact and rugged design with an integrated 4.3-inch touchscreen. The PWT 100 is the successor of the PWT 10, PWT 17, and PWT 18 series, yet offers significantly greater functionality, which is continually being extended through firmware updates.

PWM 21: the inspection unit with especially tight measuring tolerances
The PWM 21 features particularly low measuring tolerances, the ability to be calibrated, and a very wide range of functions. Beyond being used for the commissioning and functional testing of encoders, the unit can also be utilized for diagnostics in a closed control loop. In conjunction with the ATS software, the PWM 21 is a complete adjustment and testing package. Its functionality includes a connection dialog, extensive position displays, diagnostic functions, assistance for mounting and testing, and the display and alteration of memory contents.

Interesting offers regarding testing and inspection equipment
Specialists for repairs and maintenance can learn how to use the PWT 100 and PWM 21 testing and inspection equipment in the “Encoder Diagnostics MG-DIAG” course at the HEIDENHAIN training center. That way, companies will have their own testing and inspection specialist on-site. Companies that don’t want to train their own specialists can turn to the HEIDENHAIN service department or HEIDENHAIN agencies. They offer numerous adjustment, testing, and inspection services as well.

Contact person – Trade press

Uli Poestgens

Marketing Communications

+49 8669 31-3952

presse@heidenhain.de
Downloads