Press releases and professional articles for journalists and editors

HEIDENHAIN develops, manufactures, and sells components for the core industries of machine tools, electronics, and automation. We also offer extensive press information for other product fields and industries.

Contact us directly if you have a specific question or wish to be added to our press mailing list: presse@heidenhain.de

Debut of the new OCM and grinding functions for the TNC

Optimized Contour Milling (OCM): the next generation of trochoidal milling

Trochoidal milling stands for highly dynamic milling at excellent material removal rates. Unfortunately, the tool paths involved are optimal only for grooves. At EMO 2019, HEIDENHAIN changed this state of affairs with a new option for the TNC 640, TNC 620, and TNC 320 controls. Optimized Contour Milling (OCM) allows the trochoidal milling principle to be utilized for a considerably wider range of applications. In addition to the roughing of any open or closed pocket and island, OCM also offers cycles for the finishing of pocket floors and side walls.

As is the case with trochoidal milling, OCM limits the wrap angle and permits milling along the entire cutting edge. With OCM, the user can program any contour on the TNC 640 as usual from the shop floor. The control then automatically calculates the optimum tool paths for holding the cutting parameters constant. The subsequent machining operation runs with continuously optimum cutting values, resulting in increased machining speed and a noticeable reduction in tool wear.

A sample part presented at EMO showed just how effective the new milling strategy is. For our sample workpiece at the tradeshow, OCM lowered the machining time and tool wear by a factor of three compared with conventional milling strategies.

Grinding: achieve perfect finishes in a single setup

The TNC 640 was already able to handle milling and turning operations in a single setup. But at EMO, HEIDENHAIN showed that the control can master a third production process for the complete machining of a workpiece; namely, jig grinding. Having a milling, turning, and grinding package on a single machine offers many benefits, particularly for quality-intensive industries such as mold making and medical technology. These industries can now machine parts to exceptional surface quality in a single clamping.

The new functions enable the jig grinding of any contour on a milling machine. In addition, easy-to-use standard dressing cycles on the TNC 640 can true up grinding tools inside the machine tool. The standardized operating design for milling, turning, and grinding makes usage particularly easy. What’s more, optimized tool management for every process supports the user with both grinding and dressing.

Downloads
Press release